Signal Integrity

Power-aware Signal Integrity and EMI/EMC On High-speed Digital Chip-to-Chip Links

Signal Integrity header image 2

Workflow with IBIS Models

Posted July 30th, 2008 · 2 Comments · Video

Share

IBIS (Input/Output Buffer Information Specification) is a behavioral modeling specification for characterizing the inputs and outputs of integrated circuits. This 7 minute video shows how to use them in a signal integrity workflow. The ADS Transient-Convolution Simulator is used to determine the eye diagram and jitter decomposition from a schematic that includes IBIS models from two semiconductor companies (Xilinx and Micron in this example) joined with a channel model consisting of traces and vias.

IBIS Models in ADS

Anders Ekholm, the Librarian of the IBIS Committee, maintains an IBIS Model Suppliers directory.

Teraspeed Consulting IBIS Resource page also has a comprehensive list of models and all things IBIS.

Tags: ·····

2 Comments so far ↓

Leave a Comment