Signal Integrity

Power-aware Signal Integrity and EMI/EMC On High-speed Digital Chip-to-Chip Links

Signal Integrity header image 2

ADS DesignGuides and DesignKits

Posted June 15th, 2010 · 2 Comments · Workshop

Share

Post updated with ADS 2011 DesignGuides, November 23, 2011

Post updated with new UHS-II DesignGuide link, October 22, 2010

Here’s a list of our ADS high speed digital DesignGuides on the EEsof Knowledge Center.

Note: Access to these requires an active license and Knowledge Center login:

ADS 2011

ADS 2009 Update 1

  1. Signal Integrity Design Using Channel Simulation and EM Co-design (workshop/seminar materials, requires ADS and EMPro for some examples)
  2. PCI Express® DesignGuide (only requires ADS)
  3. HDMI DesignGuide (only requires ADS)
  4. USB DesignGuide (only requires ADS)
  5. DDR DesignGuide (only requires ADS)
  6. New! UHS-II (only requires ADS)

PCI Express is a registered trademark of the PCI-SIG.

In addition, you can download the ADS DDR2 and DDR3 Compliance DesignKits from the bottom of this page: http://www.agilent.com/find/eesof-ads-latest-downloads. DDR2 and DDR3 are labeled DDR2 CM Toolkit, V1 and DDR3 CM Toolkit, V2, respectively. Also, the docs for the DDR2 and DDR3 Compliance DesignKits are here: DDR2 Compliance DesignKit doc and DDR3 Compliance DesignKit doc

What’s the difference between a DesignGuide and a DesignKit? Both extend ADS into specialized areas. A DesignGuide is a simply project template, whereas a DesignKit adds specialized functionality.

Tags: ·

2 Comments so far ↓

Leave a Comment