Signal Integrity

Power-aware Signal Integrity and EMI/EMC On High-speed Digital Chip-to-Chip Links

Signal Integrity header image 2

The Perils of Modeling Distributed Structures as Lumped Elements

Posted June 3rd, 2011 · Please leave a comment · Article

Share

Lambert Simonovich

Lambert Simonovich, founder and president of Lamsim Enterprises Inc., has posted a nice article on the perils of modeling distributed structures (vias in this case) as a single lumped element (a capacitor in this case). The lumped element approximation works if the total delay across the via is much less than the rise time of the edge, but not otherwise. He gives an example of such a model that worked at 3.125 GB/s but which fails at 10 GB/s. The title of the article is PCB Vias Are Capacitive But Not Necessarily Capacitors and Bert uses the distributed and lumped element models in ADS to illustrate his point. Thanks, Bert!

Bert sent me pointers to some other work too. I thought I’d pass those along too:

Tags:

Please leave the first comment so far ↓

Please leave the first comment.

Leave a Comment