Signal Integrity

Power-aware Signal Integrity and EMI/EMC On High-speed Digital Chip-to-Chip Links

Signal Integrity header image 4

Entries Tagged as 'IBIS'

Time-aligning Your IBIS AMI_GetWave Function

January 23rd, 2013 · No Comments · Application Note

Share
By Colin Warwick There are two kinds of eye diagram metrics: those that just look at the received waveform (e.g. “density plots”) and those that compare the received waveform to the correct, transmitted bit pattern (e.g. BER contour, bathtub plots). For the latter type to work properly, the Channel Simulator and the models must works […]

[Read more →]

Tags: ···

Four Things That Drove Me Nuts About IBIS 5.1

September 25th, 2012 · 6 Comments · Technical Paper

Share
Here are a few of the things that tripped me up when I first started to learn about IBIS 5.1.

[Read more →]

Tags: ··

Efficient End-to-end Simulations of 25G Optical Links

May 11th, 2012 · No Comments · Presentation

Share
You can now build and run mid-channel repeater and opto-link models with SystemVue and ADS using an extention of the IBIS format.

[Read more →]

Tags: ···