Signal Integrity

Power-aware Signal Integrity and EMI/EMC On High-speed Digital Chip-to-Chip Links

Signal Integrity header image 4

Entries Tagged as 's parameters'

The Power of S-parameters for High Speed Digital Design

May 29th, 2012 · 10 Comments · Conference

On-demand version of tutorial introduction to s-parameters for high speed digital design. Original in-person tutorial was at IEEE International Symposium on EMC 2012.

[

Tags: ··

Kramers-Kronig in Pictures

December 10th, 2009 · 1 Comment · Application Note

Posted by Colin Warwick The real part of the frequency response comes entirely from the even part of the time response. Fangyi Rao and I recently wrote an article for EE Times’ RF Design Line about our patented method of creating causal time domain models from bandlimited s-parameters. The title S-parameters without tears is homage […]

[

Tags: ······

S-Parameter Bisection Using Optimization Techniques

November 12th, 2009 · 11 Comments · Application Note

An optimization-based methodology to bisect an arbitrary set of S-parameters into two equal half using Agilent’s Advanced Design System (ADS).

[

Tags: ·····